ATI Industrial Automation   ATICombinedDAQFT .NET Class Library  

Visit our website.

GetMaxLoad( axisIndex as Integer ) As Double

Get the maximum load of an axis.

Arguments

axisIndex

In: The index of the axis to find the maximum load of. 0=fx,1=fy,2=fz,3=tx,4=ty,5=tz.

Returns

The maximum rated load of the specified axis, in the current output units, or 0 if the calibration has not been initialized by calling LoadCalibrationFile.

See Also

LoadCalibrationFile